Avnet Abacus is an authorised Yageo distributor throughout Europe.
Established in 1977, the Yageo Corporation has become a world-class provider of passive components services with capabilities on a global scale, including production and sales facilities in Asia, Europe and the Americas. The corporation provides one-stop-shopping, offering its complete product portfolio of resistors, capacitors and wireless components to meet the diverse requirements of the world of technology. Yageo currently ranks as the world No.1 in chip-resistors, No. 3 in MLCCs and No. 4 in ferrite products, with strong global presence. Yageo’s product offerings are targeting at key vertical markets, including consumer electronics, computers & peripherals, industrial, alternative energy and automotive.
YAGEO XSemi Power MOSFETs feature low on-resistance and high switching speed and are widely used in almost all electrical and electronic systems. Building on a track record of shipping billions of devices, YAGEO offers a broad portfolio of low, medium, and high voltage MOSFETs to serve the needs of customers for highly efficient and compact solutions. YAGEO XSemi is the new YAGEO semiconductor brand. | ![]() |
- In December 2018, the YAGEO Corporation acquired Pulse Electronics.
- In June 2020, the YAGEO Corporation acquired KEMET.
- In March, 2023, they also acquired Heraeus Nexensos which became YAGEO Nexensos.

EV charging infrastructure solutions
Discover Yageo’s range of passive devices for EV charging infrastructure including, EMC components, circuit protection, sensors, DC-link capacitors, and transformers.
Learn More
Yageo products and solutions
Learn more about the latest products and solutions from Yageo: SEE ALL

Ask an expert
Have a question? Our regional technical specialists are on hand to help.
Documents
Legal documents
Yageo
CQ series MLCCs
The CQ series of MLCCs for high frequency applications from Yageo has excellent temperature characteristics, a narrow tolerance of capacitance and even lower ESR, ESL, and dissipation factor than the standard NPO.

Yageo
AS series automotive grade X7R MLCC
The AS series is an automotive grade X7R MLCC with soft termination, manufactured with continuous quality improvements and assurances to further solve the cracking issue caused by excessive mechanical stress and thermal fatigue.

Yageo
AC series
Yageo AC series automotive grade chip resistors feature superior resistance against sulfur containing atmosphere, halogen free epoxy, and MSL class I.

Yageo
AC series automotive grade MLCC
Yageo's AC series automotive grade MLCC is AEC-Q200 qualified as well as MIL-STD-020D tested to ensure its reliability under various temperatures and humidity conditions and still possess long endurance.