Mission-Critical and Non-Mission-Critical PSU | Avnet Abacus
Mission-Critical and Non-Mission-Critical PSU | Avnet Abacus

Meeting regulatory requirements for mission-critical and non-mission-critical rolling stock power supplies

All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel

The regulatory requirements surrounding mission-critical and non-mission critical rolling stock power supplies are paramount to application safety, but ready made solutions are available to meet these complex standards.

The railway industry is continuing to grow at least as fast as it has done in recent years, with brand new infrastructure projects rolling out all over the world. The market for new rolling stock in rail, suburban rail, metro and tram projects is also growing following high levels of investment in Europe, the Americas and Asia, with huge quantities of trains set to be built in Europe alone over the next few years. A considerable increase in passenger numbers is expected. Alongside brand new carriages, there is also a growing trend for adding retrofitted passenger comfort systems such as LED lighting, infotainment and connectivity systems to existing rolling stock. Both of these trends are resulting in increased demand for railway compatible power supplies.

All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are of course no exception. Ordinary industrial or high reliability power supplies cannot be used in this heavily regulated sector; the demands are so challenging and so specific that specialist power supplies designed and built only for railway applications must be used. These power supplies are specially designed to comply with the relevant European or worldwide railway systems standards and, in most cases, traditional brands with long histories, traceability, and qualified production are used by railway equipment manufacturers. 

Figure 1: Examples of mission critical applications

 

Power supply applications in trains can broadly be split into mission-critical and non-mission critical. Mission-critical power systems (see figure 1) power traction subsystems and braking subsystems. These power supplies require the highest possible reliability since there are heavy financial penalties for operators if trains break down, blocking the tracks, and obviously the safety implications of a brake failure are extremely severe. Non-mission-critical applications (see figure 2) cover practically everything else on board a train carriage, from the passenger WiFi routers to the air conditioning and security cameras. These non-mission-critical applications can include sensitive electronics with complex power supply needs, such as CPUs and sensitive analogue circuitry.

Perhaps surprisingly, all rolling stock electronic equipment, from braking systems to LED lighting, must meet the same European quality standard, EN50155. Replacing older standards such as the UK’s BRB/RIA standards and the French NF F 01-510 standard, the European EN50155 is actually an umbrella, referring to various other standards where necessary to define the environmental conditions that power supplies must operate in as well as specifying electrical and mechanical performance parameters.

Rail power supplies experience a wide range in input conditions – amongst the most challenging for any industry – including brownout operation, transients and spikes. Power comes from batteries located at the front or rear of the train and travels long distances down cables, which make it susceptible to interference. Since the same batteries are also used to power high power loads such as starter motors, the supply can fluctuate surprisingly large amounts.

Figure 2: Examples of non-mission-critical rail applications

EN50155 defines nominal input voltages as 24, 48, 72, 96 and 110V; 110V is the voltage output from the train’s lead acid batteries, and the other figures represent common power bus voltages found in trains (there are railway power supplies on the market that can accept an input voltage range of up to 10:1, wide enough to cover all these nominal values, such as the Bel Power HP series). The continuous input voltage range required is between 0.7x to 1.25x nominal. Short-term fluctuations need to be allowable for a brownout level of 0.6x nominal for 100ms, and a transient level of 1.4x nominal for 1s. In practice, this means equipment should be ready to deal with the full 0.6 to 1.4x input voltage at all times as the regulations strictly prohibit any deviations in the output.

EN50155-compliant power supplies also have to be able to produce an output despite total interruptions of up to 10ms in the input voltage. This is typically achieved using bridging capacitors at the input. These capacitors also perform a smoothing function, helping the power supply to deal with the required DC ripple factor of 15% of nominal input voltage, though a diode is also required for reverse polarity protection, which also smooths the input.

EN50155 is also very strict on EMC, ESD and transient requirements, referring to EN50121-3-2. The latest version of this standard extends its radiated emissions scope up to 6GHz to avoid interfering with new short-range wireless standards in the 5GHz band. ESD discharge levels by direct contact or through the air are defined, as well as the limits for surges and fast transient bursts.

The environmental parts of the standard are just as stringent. There are four operating temperature classes that power supplies can conform to, with -40 to +70°C being the most stringent. They are also expected to withstand an extra 15°C overtemperature condition for 10 minutes using only baseplate conduction/convection cooling. Humidity levels and shock and vibration requirements are also covered by referring to EN61373.

Since all power supplies, mission-critical and non-mission-critical, must conform to EN50155, a system designer working on, say, a 100W LED lighting retrofit system is faced with choosing a power supply with similar performance levels, reliability and longevity to the systems intended for powering the braking and control systems. These power supplies are manufactured to last 20 years minimum (MTBF in excess of 1 million hours) and they have a premium price tag to match. For a simple cabin lighting application, this would be overkill to say the least, but until recently rolling stock system designers had no other option.

To meet the needs of non-mission-critical applications like interior LED lighting in railway rolling stock, Bel Power has developed a series of new chassis mount power supplies under its well-known Melcher brand which is considerably more cost effective than a traditional railway power supply, while still fully complying with EN50155. Despite more cost effective construction and the use of components that wouldn’t be found in a traditional railway power supply such as electrolytic capacitors, the RCM series (see figure 2) meets every part of EN50155 while maintaining a good DMTBF (demonstrated mean time between failures) of >300k hours.

The RCM series comes in four models. The 500W and 1000W units are primarily intended for 110V applications, while two smaller models, 150 and 300W, have a wider input range covering all the nominal input voltage levels specified by EN50155. Outputs are 12 or 24V, ideal for LED lighting, infotainment systems, signage, WiFi routers or cellular repeaters, and any new or retrofitted application that doesn’t need the extreme longevity of mission-critical systems. All four models in the RCM series are quick and easy to mount; they can be mounted vertically or horizontally to a chassis or the wall with just four screws, perfect for retrofit applications.

The RCM series can operate at ambient temperatures between -40 and +70°C (EN50155 class TX) without any derating, using only convection plus conduction cooling through the mounting area. EN50121-3-2’s EMC requirements can be met without the need for additional external filtering components. Other features include OUT_OK and remote ON/OFF signals for remote monitoring and control.

As rolling stock around the world is upgraded to meet modern expectations of passenger comfort levels, features such as infotainment, aesthetically pleasing LED lighting and passenger communications repeaters are being widely installed. The complexity of these systems means decentralised power architectures are becoming more prevalent in rolling stock. In addition to the RCM series, Bel Power Solutions' portfolio of products includes a broad range of power supplies specifically designed for railway applications. Click below to visit our railway power solutions page and download the brochure. Our Europe-wide team of field application engineers has a deep knowledge of these modern systems and can help you select the appropriate power supply for your designs - Visit the Ask an Expert page to get in touch.

Want more like this? Sign up for our newsletters

About Author

Philip Lechner

Philip Lechner studied electronics and telecommunications in Amsterdam before beginning his career i...

Mission-Critical and Non-Mission-Critical PSU | Avnet Abacus
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Mission-Critical and Non-Mission-Critical PSU | Avnet Abacus
Related Articles

No related articles found

Mission-Critical and Non-Mission-Critical PSU | Avnet Abacus
Related Events
Related Designs Menu