what-is-polarization-keying-and-color-coding-for-interconnect
what-is-polarization-keying-and-color-coding-for-interconnect

What is polarization, keying and color coding for interconnect?

electric vehicle dashboard

Establishing a properly aligned connection quickly is key in any assembly or installation process.  Polarization, keying and color coding are primary means to ensuring connections are made quickly and safely.  In this article we’ll discuss each of these means and the advantages of them.

What is Keying?

Many connectors are designed with a means of being “keyed”, but what does this really mean and what is it designed for?  Keying is an important feature because it prevents mis-mating.  Incorrect mating could result in mechanical damage, lost signals, or even a short circuit, resulting in lost.  Resulting in lost time for troubleshooting and possibly damaged equipment.  Connector keying is the primary means of combating these situations by ensuring the connectors can only be mated in one direction.  Keying takes different forms such as a rectangular connector with a blanking pin in one position or a circular connector with a notch to ensure proper alignment of all pins such as the Molex BradPower D-Size connectors.

Polarization

Polarization preventss mis-mating by allowing only one orientation to connect which is especially important when the operator is unable to see the connector parts while uniting them, or “blind mating”.  The Molex polarized Saber Power connector ensures the proper orientation is easily achieved.  The image below illustrates how the shape of each position of the receptacle ensures proper polarization.

Color Coding

In a situation where there are several connectors that look similar, color coding helps the operator identify the proper connections quickly, saving time in the assembly or installation process.  Examples can be seen in common connectors such as the audio video RCA cables where red, white and yellow indicate right and left channel audio and video, or the Molex CP Wire to Board connectors where each color is for a specific signal or voltage.

Conclusion

All three of these concepts are relatively simple, but provide a crucial means of safety, speed and structure in assembly and installation.  While polarization and keying are commonly confused, you can see how each serves a specific purpose.  Keying can add bulk to a connector but provides a physical attribute, polarization ensures each contact is connected with the proper mate and color coding provides a quick visual indication for proper connection without adding bulk.

Our technical experts at Avnet are here to help you choose the right solution for your application.

 

關於作者

Jamie Pederson

Jamie Pederson is a Technical Content Manager with Avnet. He has 18 years of electronics industry ex...

what-is-polarization-keying-and-color-coding-for-interconnect
Related Content
Molex campaign, electric vehicle dashboard
 
 
Increased demand for ADAS and autonomous driving are pushing automakers to add more electronic control units and next-gen domain control units to vehicles resulting in a need for reliable interconnect solutions in harsh environments.
 
what-is-polarization-keying-and-color-coding-for-interconnect
相關文章
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
4D雷達:ADAS領域的新一代感知神器
2024年8月15日
高速NOA、環線NOA甚至城市NOA的不斷普及,顯示L2+大範圍落地的趨勢正在加速。實現NOA的三種主要傳感技術(攝影鏡頭、毫米波雷達和雷射雷達),三種解決方案各有優劣,能夠互補。
Conceptual image of smart car in purple
完善充電基礎設施建設,引領可持續技術發展
2024年5月15日
充电基础设施作为电动汽车的“能量补给站”,其技术深度与成熟度直接关系到电动汽车的推广与应用。
what-is-polarization-keying-and-color-coding-for-interconnect
相關活動

未找到相關活動