Explore Renesas´ vast array of wireless technologies designed to revolutionize the way you connect and communicate with the world. The advanced wireless solutions seamlessly integrate with their cutting-edge MCUs and MPUs, ensuring reliable connections for a wide range of applications. From smart homes to health and fitness technology, tracking systems, and point of sale solutions, setting the benchmark for performance, Renesas offers industry-leading innovations including ultra-power-efficient Wi-Fi, highly sensitive and powerful NFC, and versatile Bluetooth® Low Energy SoCs. The comprehensive ecosystem provides as well an extensive toolkit for rapid evaluation and production, featuring a rich library of Winning Combinations.
- Bluetooth® Low Energy
- Wi-Fi
- NFC
Bluetooth® Low Energy
Adding Bluetooth® Low Energy (LE) capabilities to a system can be a challenging task for users new to the technology. From component selection to RF layouts and regulatory certifications, there are many jobs to be done to create an end product with the necessary wireless performance and approvals.
Using a certified module can help tremendously in this task. All of Renesas' Bluetooth LE modules come certified to regulatory compliance, Bluetooth qualification and external circuitry so customers no longer have to integrate into their product by themselves. Products marked "available" in the built-in antenna and external antenna columns of the parametric search table are provided as modular products. Renesas also provides a guideline for acquiring Bluetooth qualification for final products.
Featured products
DA14592
The DA14592 is a very low-power, BLE SoC offering M33 + M0 ARM Cortex cores supporting floating point application programming (M33) and Renesas-programmed, BLE 5.4 and capable of supporting other (proprietary), ISM band protocols. New for Renesas BLE, it includes embedded Flash and its memory (Flash/ROM/RAM) and functionality has been optimized to cost-efficiently support a broad range of BLE applications.
Read MoreDA14695
The SmartBond™ DA1469x family of Bluetooth® Low Energy solutions is a feature-rich range of multi-core microcontroller units for wireless connectivity.
The product family builds off the successes of Renesas' SmartBond line, boasting three additional cores that offer greater processing power, resources, range, and battery life, enabling developers to push the boundaries of a wide array of connected consumer applications. The DA1469x line provides developers with advanced connectivity features to future-proof their devices and fit the needs of multiple applications.
Read MoreWi-Fi
Renesas' Wi-Fi connectivity technologies deliver end-to-end connectivity solutions for both clients and access points addressing IoT, infrastructure, industrial, automotive, multimedia applications, and more.
Renesas' ultra-low power Wi-Fi solutions are designed for IoT applications where extended battery life, high RF performance, robust security, and ease of application development are key market needs. We are also an innovative leader in hardware and software technologies and offer a broad range of Wi-Fi generations. Renesas' rich Wi-Fi portfolio includes highly integrated Wi-Fi 4, 5, and 6 chip solutions including the new 6GHz extension "6E".
Featured products
DA16200
The DA16200 system-on-chip (SoC) is the world's first Wi-Fi SoC to deliver year-plus battery life for always-connected Wi-Fi IoT devices. DA16200 is a low power Wi-Fi networking SoC that delivers a dramatic breakthrough in battery life even for devices that are continuously connected to the Wi-Fi network. In most applications, one year plus battery life is achievable. There is no tradeoff in output power or range, as the SoC's range is industry-leading.
Read MoreDA16200MOD
DA16200 modules are the perfect complement to the DA16200 ultra-low power Wi-Fi SoC. They deliver the same long battery life and low power consumption but in a convenient form factor. The modules are complete with all required components and are regulatory certified by the FCC, IC, CE and other regulatory bodies.
Read MoreDA16600MOD
The DA16600 modules provide a convenient way to add both low power Wi-Fi and low power Bluetooth® Low Energy (LE) functionality to your device. The low power Wi-Fi DA16200 system-on-chip (SoC) and the low power Bluetooth LE DA14531 SoC are integrated together on a single module. Together, they deliver long battery life and low power consumption in a convenient form factor.
Read MoreNFC
Renesas' ground-breaking Near Field Communication (NFC) technology and products have been developed since 2014, targeting the most demanding applications in high-growth markets such as NFC wireless charging, mobile, and point of sale (PoS). Manufacturers of the latest mobile and wearable devices are keen to replace wired charger connections with wireless charging, because of its convenience, design flexibility and reliability benefits. From passport control kiosks to consumer goods, from gaming consoles to check-in counters, from printers in your office to manufacturing automation, from small mobile Point of Sale terminals to Smart PoS – NFC is an inseparable part of your daily experience.
Featured products
PTX100R
The PTX100R NFC reader serves IoT and Point-of-Sale (PoS) applications, implementing a unique sine wave hardware transceiver architecture and offering a winning combination of superior transmit power and sensitivity, accurate wave shaping, and a reduced bill-of-materials compared to conventional square-wave NFC controllers – products which have changed little over the past decade.
Read MorePTX105R
The PTX105R is the industry’s best-performing NFC controller for Internet of Things applications. Due to its unique sine wave architecture, PTX105R is an optimized solution for IoT applications with small form factors. Superior sensitivity, accurate digital wave shaping, and a reduced bill-of-materials compared to conventional square-wave NFC controllers enable optimal interoperability, simplified FCC certification and faster NFC Forum compliance.
Read MorePTX130R
The PTX130R NFC reader IC featuring native support for the Android™ operating environment provides an ideal way to add NFC communications capability to embedded computing systems built around a touchscreen display. The PTX130R features a very high RF output power of up to 2W at the antenna, providing robust connectivity and enabling OEMs to achieve compliance with the strict requirements of the EMVCo standard for payment card transactions even when operating via an antenna that is placed close to or behind a noisy display.
Read MoreRenesas Wireless Connectivity Solutions
Simplifying the connected future: Navigating complexity in the IoT landscape with Renesas Wireless Connectivity

Have a question? Contact usEmail: |