Custom Meta Tags
Hero Banner
Sub Navigation
Title (LC)

IoT Cloud Security: The Missing Link in IoT Success

Intro (MM)

The cloud is a defining aspect of the IoT and has a pivotal role in connecting, collecting, storing, and analysing data from the large numbers of deployed endpoint devices. While the migration of certain functions into the edge can reduce latency, lower power consumption, and mitigate privacy risks, the cloud provides a scalable and secure platform to aggregate and store the massive volumes of data generated by IoT devices. Instead of relying on individual devices to process and store data locally, this centralised resource allows for efficient data management and ensures that valuable information can be accessed and analysed from anywhere at any time.

The cloud's scalability is particularly crucial in the context of IoT. As more and more devices are connected, the cloud provides the infrastructure to handle the exponential growth of data. Its computational resources can accommodate the dynamic nature of IoT and scale up or down based on demand. This ensures that IoT systems can accommodate millions or even billions of devices, enabling organisations to leverage IoT data at scale.

IoT Cloud Security
Narrow LC (LC)

IoT in the Cloud

The cloud is the home of vast data storage and powerful computing, often boosted with accelerators containing specialised processors such as graphics processing units (GPUs) or custom field-programmable gate arrays (FPGAs) configured for efficient execution of AI applications. This provides a platform for database tools, analytics applications, and machine learning algorithms that enable organisations to extract actionable insights from the massive influx of IoT data. These can be delivered through web, desktop or mobile applications - which could be from the cloud provider, IoT integrator, or can be third-party applications – designed to help users visualise and assimilate the information. Ultimately, the insights enable businesses to make data-driven decisions, enhance operational efficiency, and create innovative new products and services.

The cloud can be a private resource or provided through an independent service provider. Some well known providers include AWS, Microsoft, and Google.  There are also specialist software developers that make tools available on a software as a service (SaaS) basis, and IoT solutions providers that may provide a selection of applications termed platform as a service (PaaS).

WISE PaaS Architecture

Figure 1: IoT cloud platform as a service (PaaS)(Source:Electronics360).

Figure 1 illustrates an established PaaS architecture, which can be hosted on private or public cloud resources. Software techniques such as containers can facilitate moving IoT workloads from the cloud into edge devices, and may be supported as part of managed cloud services or implemented with third-party software based on frameworks like Kubernetes or Docker.

IoT Cloud Architecture

Figure 2. Data enters the cloud from various sources and flows through various layers that handle ingestion, processing, storage, and interface with downstream apps (Source:Embitel).

Layered Cloud Architecture

Another view describes the cloud architecture in terms of the dataflow through ingestion, processing, storage, analytics, and exporting to end-user applications. Figure 2 shows the various layers involved in supporting the exchange and processing of data.

The cloud platform needs to be architected to allow different devices to connect, handle all the incoming data in its various forms, apply the appropriate processing, and store the data in a way that allows analytics applications to retrieve the data and add value.

Underlying everything, the cloud part of the IoT implementation is responsible for collecting, organising, and analysing the data received from IoT “things” – the perception layer, as described in the first article of this series – whether filtered or not by aggregators and processors in the edge layer. The way this data is organised and analysed can depend on the nature and source of the data, and on the insights sought from analysis.

IoT Support (CO)

We understand that the IoT can be overwhelming, so if you need support with your next IoT project or IoT security in particular, why not get in touch with our experts? Our IoT, Wireless and Connectivity teams are on hand to help you with your next IoT challenge.

Learn More
Secure Provisioning (GBD)

Security

Secure Provisioning

Services providing keys and certificate injection into Secure Elements or MCU for full end-to-end Security.

Main body and conclusion (LC)

For example, handling data from industrial equipment is collected, and the computing applied to calculate appropriate performance metrics, demands a different approach compared to interacting with a fleet of vehicles. Cloud providers may offer a selection of managed services that can be tailored to specific customer requirements. There is also a vibrant market for third-party software specialised in data ingestion, preparation, storage, and analytics.

An internal aggregation layer may be implemented to bring together data from various sources. An ingestion framework may then be used to direct the data into a processing layer. The processing layer can be organised in various ways: a three-stage approach may accept raw data from the ingestion layer, apply techniques such as machine learning to further refine the data, and finally present usable data to analytics applications that generate actionable insights for purposes such as automating industrial processes, driving business decision making, directing new product development.

A final outbound, or storage layer can provide services such as APIs and managed access that make information available to downstream applications.

Security in the Cloud

Security is a critical aspect of the cloud's role in IoT. The cloud provides robust security measures to protect sensitive IoT data from unauthorised access, ensuring data integrity and confidentiality. Additionally, the cloud's centralised security infrastructure allows for efficient monitoring, threat detection, and rapid response to potential security breaches across the IoT ecosystem.

The cloud platform relies on strong authentication mechanisms, such as cryptographic keys, digital certificates, and multifactor authentication, to verify the identity of IoT devices and ensure that only authorised devices can access services. Role-Based Access Control (RBAC) and fine-grained authorisation policies restrict access to specific resources and actions based on device roles and permissions.

Further security techniques include using secure communication protocols, such as Transport Layer Security (TLS) or Datagram Transport Layer Security (DTLS) to encrypt data transmitted between IoT devices and the cloud. Encryption ensures that data remains confidential and cannot be intercepted or tampered with during transmission. Additionally, secure communication protocols provide mechanisms for endpoint authentication and protection against man-in-the-middle attacks.

Data encryption is also employed to protect IoT data at rest in the cloud, such as when stored in databases or file systems. This helps to prevent unauthorised access even if the storage infrastructure is compromised. Proper encryption key management practices, including secure key storage and rotation, are needed to maintain the confidentiality of encrypted data.

In addition, cloud-based security tools and services, such as intrusion detection systems (IDS) and security information and event management (SIEM) solutions, are used to monitor network traffic, detect anomalous behaviour, and identify potential security threats in real-time. These tools employ machine learning algorithms and behavioural analytics to identify patterns or indicators of malicious activities and trigger appropriate responses.

In the cloud, it is also possible to use advanced analytics techniques including artificial intelligence to identify security risks, detect anomalies, and uncover potential data vulnerabilities. AI can detect patterns and predict threats to enhance security posture and response.

Cloud IoT platforms often provide security auditing capabilities to monitor compliance with security policies, regulations, and industry standards. Auditing helps identify security gaps, track security events, and maintain an audit trail for forensic analysis and compliance reporting purposes.

There are also incident response mechanisms including incident management workflows, automated responses, and recovery processes. These are essential for promptly addressing security incidents, while incident response plans can guide mitigation, recovery, and investigation if a security breach occurs.

In addition, physical security measures at the data-centre premises, such as access control systems, video surveillance, and environmental controls are, of course, essential.

Conclusion

The cloud has a central role in any IoT solution, as the convergence point for data from multiple sources, not only sensor data but also any other relevant data from third-party feeds. Broadly, applications in the cloud are required to collect, organise, and analyse the data. In practice, there are many ways to approach this, depending on the types of data and their sources, and the insights required from the analysis. Several layers may be implemented to ingest, prepare, store, and analyse the data, typically accomplished by selecting managed services from cloud providers or using third-party software.

Some of the cloud’s vast processing power must be directed towards robust security, to protect services and data against threats such as unauthorised access, tampering, and data theft, and so preserve trust, reliability, and confidentiality.

More from this series:

IoT Security Authors (LC)

About Author

 

EMEA IoT Security Experts

We use 'EMEA IoT Security Experts' as a collective byline when our team of IoT Security experts and writers collaborate on content.

 

PDF article pages (MM)

All IoT Security articles in one place...

What happens when the devices we depend on become our greatest vulnerabilities? As the Internet of Things (IoT) continues to surge in both range and frequency of use, with billions of devices connecting our homes, workplaces, and cities, the same technologies that make our lives more efficient also introduce unprecedented risks. Securing this intricate web of communication isn’t just a technical challenge — it’s a matter of trust, safety, and resilience in an increasingly connected world.

Download the full PDF today to access all of our IoT Security Series articles in one place for convenience and read them at a time that suits you. This PDF also includes an overview of the current state of IoT security and what to expect in the next decade.

IoT Security Series PDF front cover
PDF download (MFUR)

Fill in the short form below to start your PDF download.

 
Your download will start in {seconds} second(s). If your download doesn't start <a href="{url}" target="_blank">click here</a> to download.
 
Secure elements (GBD)

Security

Secure Elements

Hardware Root of Trust used for crypto operations and key storage.

Secure Library (GBD)

Security

Secure Library

Software Root of Trust integrated into any MCU/MPU used for crypto operations and key storage.

Secure MCU (GBD)

Security

Secure MCU

MCU with built in security features and key storage.

IoT Overview (GBD)

Service

See IoTConnect

The IoT can be overwhelming. You need to leverage new technologies like AI, deep learning and data mining to make the most of your investment. Let us help you.