IoTConnect® is the fastest and most scalable way to securely connect your connected products to the cloud. Avnet has partnered with both Amazon Web Services and Microsoft to offer IoTConnect on AWS IoT and Microsoft Azure.
Avnet is working with the industry’s leading semiconductor vendors to enable IoTConnect to work with the most advanced, powerful, and fully-featured microcontrollers available today. It is now easier to experience, first hand, how IoT connectivity can take your product to the next level.
Avnet’s engineers have created a variety of guides to quickly demonstrate IoTConnect on some of the latest IoT development kits and evaluations boards from our supplier partners. By following these quick start guides, you can get connected in minutes, not hours.
You won’t need to sign up to a cloud service, you won’t need to configure a toolchain, and you won’t have to write a single line of code. If you prefer compiling code from source, check out the Developer Guides to quickly get your developer environment setup and begin building your application.
IoTConnect Guides are available today on the following development kits:

ST Discovery 套件(基于STM32U5 系列,用于IoT节点)
这款开发工具包具有Wi-Fi、蓝牙和多种传感器,并支持通过Arduino、STMod+和Pmod™接口进行扩展。工程师可以使用这款套件开发互联装置,如可穿戴传感器,以及智慧家居或智慧工业应用。
了解更多Microchip WFI32-IoT 开发板
这款开发板具有PIC32MZ-W1 Wi-Fi模块,带有PCB天线和Trust&Go硬件安全功能。它具有额外的接口,包括MikroBUS™,使开发者能够快速添加传感器。因此,这款IoT开发平台备受青睐。您可以使用板载温度传感器和光传感器,快速创建一个智能监测解决方案。
了解更多安富利MaaXBoard SBC(基于恩智浦i.MX 8M)
这款基于恩智浦i.MX 8M处理器的SBC,非常适用于边缘智能装置。它提供了在地处理视频和音讯的能力,并支持高级操作系统(Android、Windows 10 IoT Core、Linux)。
Renesas CK-RX65N云套件(基于RX65N MCU组)
这款套件集成了RX65N MCU与LTE Cellular CAT-M1模块和以太网连接模块。有了IoTConnect的支持,几分钟内就可以将现场捕获的数据发送到云端。
Infineon XENSIV套件(带PAS CO2传感器)
XENSIV™互联传感器套件是电池供电的IoT装置的理想选择。它体积小巧,但效性强大。这款套件具有Wi-Fi和蓝牙连接功能,内置CO2传感器和OPTIGA™ Trust M安全装置。这款套件与IoTConnect安全装置管理功能配合使用,
提供了对端到对端的安全IoT连接。