Custom Meta Tags
EBV - Automotive Hero Banner (HB)

Automotive

EBV - Automotive NEW Sub Navigation
EBV - Automotive Sensors and Imaging Main Title

Automotive Sensors & Imaging technology

EBV - Automotive - Sensors and Imaging Intro (MM)

There is a huge variety of sensor devices being integrated into modern vehicle models - and these reflect the underlying trends that are now defining the automotive sector.

The first of these is increasing levels of vehicle autonomy. For on-board computing systems to be able to take responsibility for driving and react to situations that occur on the road, they need to be supplied with data from a multitude of different sources. This is leading to greater reliance on cameras - with the number of them being installed into vehicle designs expected to grow significantly over the course of the coming years. As well as conventional visual imaging, the automotive industry is now embracing the use of 3D imaging. This is set to enable detailed renderings of the environment around the car - providing full awareness of the proximity of obstacles, pedestrians or other vehicles.

EBV - Automotive - Sensors and Imaging Technology Static HTML

Also relating to autonomous driving, there is the need for inertia measurement units (IMUs). These are multi-axes devices that can deliver constantly updated parametric data on the angular orientation, velocity and direction of a vehicle. This is vital in situations where satellite navigation is interrupted, due to the vehicle entering a tunnel, a multi-storey car park, or moving between tall buildings.  

The next trend that must be outlined is x-by-wire. This is allowing mechanical systems, such as the steering column, throttle, and brake, to be replaced by electronic hardware - with benefits being derived in terms of reduced weight, less space being taken up and greater operational reliability. The movement of pedals and the vehicle’s steering wheel need to be accurately determined. This can be achieved via high resolution linear and rotary magnetic sensors.

Use of optical ToF sensor technology within the cabin will enable the monitoring of vehicle occupants. Through this, better airbag deployment may be actioned by firstly establishing if a specific seat is occupied, then judging the size of the person in that seat so that the speed/strength of deployment is appropriate. Also, the attention of the driver can be ascertained at any given time to see if they are concentrating on the road and, if not, actioning an automated response to any imminent hazard.

An ICE vehicle’s engine management system (EMS) will need to access data from temperature and pressure sensors, for performance monitoring purposes. Accurate pressure measurement enables better control of the fuel supplied to the engine, while temperature sensors can ensure that the liquid coolant is working effectively. Temperature sensing devices may also be used to check the conditions within the cylinder and the exhaust gas output. There is, likewise, a growing need for these devices within EVs. Here they are providing support to the battery management system (BMS), by monitoring the status of each of the battery cells so that potential overheating situations can be avoided.

EBV’s expansive inventory includes automotive-grade pressure sensors, TPMS devices, temperature sensors, MEMS-based IMUs, Hall sensors and CMOS image sensing devices for camera systems.

Web Content Viewer
Warning

Warning

Invalid configuration found. Contact the administrator.

 
Automotive Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Automotive Director Frank-Steffen Russ

Web Content Viewer
Warning

Warning

Invalid configuration found. Contact the administrator.

 
Web Content Viewer
Warning

Warning

Invalid configuration found. Contact the administrator.

 
Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBVchips Teaser Box (GBL) grey

Solutions

EBVchips

Semiconductor solutions developed with and for customers

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.

EBV - Automotive - Related NPI Static HTML