Heat Pumps
A sustainable, power efficient alternative to traditional heating systems
Recent energy shocks and subsequent price volatility in Europe have seen consumers and businesses seek new ways to heat their homes and premises.
Consequently, heat pumps have emerged as a highly efficient and environmentally friendly alternative to traditional fossil fuel heating systems.
By harnessing renewable energy sources like the outside air, heat pumps can significantly lower energy consumption, reduce carbon footprints, and improve bottom lines.
Indeed, the latest statistics from the European Heat Pump Association show that the market is growing fast. Around 24 million heat pumps are now installed in Europe's buildings, and the figure is rising year-on-year.
Heat pumps: Increasing popularity and efficiency
Avnet Silica's resident Power expert, Thomas Hauer delves into the world of heat pumps with Electropages, discussing their increasing popularity and efficiency compared to traditional heating methods. Heat pumps can achieve a coefficient of performance (COP) of around 4, meaning they can produce four units of heat energy for every unit of electrical energy consumed. This makes them significantly more efficient than traditional electric heaters. Additionally, heat pumps reduce reliance on fossil fuels and contribute to lower carbon emissions. They are also versatile and capable of both heating and cooling spaces. However, challenges such as inrush current and the need for complex power electronics systems present obstacles for manufacturers.
Heat Pumps: Thomas Hauer's interview with electropages
Despite these challenges, the growing demand for heat pumps, driven by rising energy costs and stricter regulations, is evident. The future of heat pumps appears promising, with advancements in technology addressing these challenges and further improving their efficiency and performance.
How do heat pumps work?
Imagine a heat pump as a reverse refrigerator.
When you put a can of soda in a fridge, it gets cold because the refrigerator extracts heat from the inside and releases it outside. A heat pump does the opposite: it extracts heat from the outside air (even in cold weather) and releases it inside your home.
Here's a breakdown:
- Heat Extraction: A refrigerant flows through a system, absorbing heat from the outside air.
- Compression: This heat-laden refrigerant is compressed, increasing its temperature.
- Heat Transfer: The hot refrigerant flows through coils inside your home, releasing heat into your living space.
- Cooling and Repeat: The refrigerant then cools down and the cycle repeats, continuously transferring heat from the outside to the inside.
Essentially, a heat pump leverages the natural heat energy available in the environment to provide warmth, making it a highly efficient and sustainable heating solution.
Many modern heat pumps are designed to be reversible, allowing you to use them for both heating and cooling throughout the year. This versatility makes them a highly efficient and convenient choice for climate control in many regions.

How heat pumps work (source: onsemi)
Featured onsemi heat pump products
Technology
Power: designing solutions with power at the core
We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Solutions
onsemi EliteSiC Solutions
Avnet Silica and onsemi are working together to deliver the SiC solutions needed to realize a greener, cleaner energy infrastructure.

PFC Controllers
Efficiency improvement and power factor optimisation. Reducing of voltage drops and current losses. Improvement by reducing harmonics and voltage fluctuations. Ensures compliance with standards, thus avoiding penalties.

Power discretes
Optimised for High temperature operation. Diodes: Low series-resistance temperature dependency. MOSFETs: Stable reverse recovery over temperature. Improved parasitic capacitances for high frequency and high efficiency application.

Gate Drivers
Gate drivers are the interface between control signals and power switches. onsemi offers broad portfolio of isolated and non-isolated drivers for a variety of power switches with advanced features to boost your system applications.

FS7 IGBT
The 1200V Trench FS7 IGBTs are newly used and recommended for the PFC stage of a three-phase heat pump system. R-series with low Vce(sat)=1.37V at rated current @25°C. Available packages: TO-247-3L, TO-247-4L, QD3, Bare die.

Working on a power project?
Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.
Like what you see?
Follow us on LinkedIn
Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.